KitKat 4.4.3 on Linux Kernel 4.1.15?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KitKat 4.4.3 on Linux Kernel 4.1.15?

586 Views
eric_reyna
Contributor II

Wondering how I could run/add the newest Linux kernel  4.1.15 for Android KitKat 4.4.3 (that currently is running linux 3.10.53) on the SabreLite board? I know it should be possible, but will NXP ever release something like that, or will I have to work on this myself? 

And if anyone has an interest, could you give me some tips/pointers on developing this (I want to start working on this, and hopefully have it done by the end of the year). 

Labels (3)
0 Kudos
1 Reply

461 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eric

I am not aware of Android KitKat 4.4 with Linux kernel  4.1.15, seems one can start with:

i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
 https://community.freescale.com/docs/DOC-95003

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos