For our project we are looking for a Freescale board with VxWorks 7 BSP and Aurora debugging interface.
The P3041DS-PC is the only board that I have found with VxWorks 7 BSP and where in the high-level description it is explicitly mentioned that it has an Aurora connector.
Is it then the standard 70-pin connector? Can I then assume that the Aurora interface is working in that board (software support in the SDK)?
Thanks a lot
Miguel
> Is it then the standard 70-pin connector
Yes, the board is equipped with standard 70-pin Aurora connector and supports Aurora (up to x2 lanes).
> Can I then assume that the Aurora interface is working in that board
Yes.
> (software support in the SDK)?
CodeWarrior supports Aurora.