AnsweredAssumed Answered

Mising port pin interrupt when switching from LLS to RUN mode

Question asked by Aleksandar Trajkovski on Jan 17, 2017
Latest reply on Jan 30, 2017 by Aleksandar Trajkovski

Hi,

I use KL05 (mkl05z8vfk4) microcontroller in LLS (Low Leakage Stop) mode.

I configured to waking up the processor from LLS with LLWU external pin PTA7 (LLWU_P3) on rising edge also I share the same pin as port interrupt pin on same edge detection.

When I trigger the pin the Cpu_OnLLSWakeUpINT() execute but port interrupt handler does not execute.

Q: Where should I share pin in processor component on Low power mode settings or in PORTA component?

Q: How to setup the pin to enable port interrupt handler execution?

 

Thanks in advance.

Outcomes