P2020 Target Board is not Booting with SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 Target Board is not Booting with SD Card

1,079 Views
nareshpuli
Contributor III

HI,

 In the  SD Card i have U-Boot and Kernel images, its working fine  , When  i  keep in NxpP2020 Target Board is not Booting with the SD/MMC Card, My thought This is hardware issue pls help how can i fix this issue .bcz when i put in another Board is Booting...

In the console it shows like this

SD boot...
Second program loader running in sram...

Regards

Naresh

Labels (1)
0 Kudos
11 Replies

625 Views
ufedor
NXP Employee
NXP Employee

The console log could indicate that the secondary program loader (SPL) is unable to properly initialize the DDR SDRAM - i.e. it is required to perform a memory test by means of a debugger or use CodeWarrior DDR Validation Tool.

0 Kudos

625 Views
nareshpuli
Contributor III

Hi ufedor,

Thanks for your information,  You said the SPL is unable to initialize the DDR SDRAM ,but In the Target Board NOR Booting is working fine,

how can we say only DDR SDRAM issue

0 Kudos

625 Views
ufedor
NXP Employee
NXP Employee

What does it mean "Target Board NOR Booting"?

Please use a debugger to check the processor state when the SD boot process stalls.

0 Kudos

625 Views
nareshpuli
Contributor III

Target Board is NxpP2020, i am getting started with this is Board, How can i check the processor state.

Regards

Naresh

0 Kudos

625 Views
nareshpuli
Contributor III

Actually we have two boards of NxpP2020,  pls  share the link  DDR Tool Download link,  where can i get 

0 Kudos

625 Views
ufedor
NXP Employee
NXP Employee

> Actually we have two boards of NxpP2020

Thoroughly check that the problem board has its configuration switches in identical positions as the working one.

> DDR Tool Download link

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to... 

0 Kudos

625 Views
nareshpuli
Contributor III

Hi ufedor,

Thanq very much

Regards

Naresh

Have a nice day.....

0 Kudos

625 Views
ufedor
NXP Employee
NXP Employee

Is the issue resolved?

Why you created two Technical Cases?

0 Kudos

625 Views
nareshpuli
Contributor III

Hi,

still it is not resolved, in the given link i  am not able to find DDR Tool, it is showing only codewarrior tools.

kindly waiting for your reply.

regards

naresh

0 Kudos

625 Views
ufedor
NXP Employee
NXP Employee

In the log:

> DIMM 0: is not a DDR3 SPD.

Try to swap DIMM modules between the working and the problem boards.

0 Kudos

625 Views
ufedor
NXP Employee
NXP Employee

> How can i check the processor state.

By establishing debug connection and examining the code being executed.

You wrote:

> when i put in another Board is Booting

Which "another Board"?

0 Kudos