MC9S12GNA16 and MC9S12GA48 in CodeWarrior v5.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12GNA16 and MC9S12GA48 in CodeWarrior v5.2

Jump to solution
644 Views
sagardhavali
Contributor III

Hello,

 

I wanted to create a new project for MC9S12GNA16 and MC9S12GA48 in CodeWarrior v5.2. I couldn't find those devices in the software.
I heard that there is a patch for it to add GNA devices but I couldn't find it anywhere. 
Can anyone help me here?

 

Thank You,
Sagar

Labels (1)
Tags (2)
0 Kudos
1 Solution
308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sagar,

About add missing device for CW v5.2, please refer to

Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method) 

or   How to install missing device to CodeWarrior for HCS12 v5.2  

Hope it helps
Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
309 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sagar,

About add missing device for CW v5.2, please refer to

Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method) 

or   How to install missing device to CodeWarrior for HCS12 v5.2  

Hope it helps
Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------