Issue in setting SSIn parent clock to PLL4 in i.MX6 4.1.15 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in setting SSIn parent clock to PLL4 in i.MX6 4.1.15 kernel

Jump to solution
1,410 Views
shabeerbadarudh
Contributor IV

Hi All,

In our custom board, we have porting linux kernel from 3.10.17 to 4.1.15.
we are facing some issues with microphone custom audio driver (chip :ICS-43432, issue : missing some samples),which is working perfectly in 3.10.17.

We have compared the audio clocks in 3.10.17 and 4.1.15, both are different. In 3.10.17 clock values IMX6_AUDIO_I2S_BCK, IMX6_AUDIO_I2S_FRCK are 3.078MHz and 48.108KHz and in 4.1.15 it is 2.88MHz and 54 KHz.

Then we have compared the clock source code in both kernel (arch/arm/mach-imx/clk-imx6q.c ) and noticed some difference. We want to derive ssi1_sel clock from PLL4. In 3.10.17 code for that configuration is present but not in 4.1.15 . So i have tried to set this in 4.1.15 kernel using the function 'imx_clk_set_parent(clk[IMX6QDL_CLK_SSI1_SEL],clk[IMX6QDL_CLK_PLL4_AUDIO])',
but it gives an error at boot time, 'failed to set parent of clk ssi1_sel to pll4_audio: -22'.

may i know the reason for these error or how do we set/configure the parent clocks in 4.1.15?

Thanks,

Shabeer

0 Kudos
1 Solution
984 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shabeer

available clock selections listed in linux/include/dt-bindings/clock/imx6qdl-clock.h,

if clock is not available one can add it using description of common linux clock framework

https://www.kernel.org/doc/Documentation/clk.txt

http://elinux.org/images/b/b8/Elc2013_Clement.pdf

example of lcd clock selection

https://community.nxp.com/thread/434986 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
985 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shabeer

available clock selections listed in linux/include/dt-bindings/clock/imx6qdl-clock.h,

if clock is not available one can add it using description of common linux clock framework

https://www.kernel.org/doc/Documentation/clk.txt

http://elinux.org/images/b/b8/Elc2013_Clement.pdf

example of lcd clock selection

https://community.nxp.com/thread/434986 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
984 Views
shabeerbadarudh
Contributor IV

Hi igorpadykov

Thanks for the response.

I have resolved my issue.

0 Kudos
984 Views
titusstalin
Contributor V

Hi Shabeer,

Can you please share me the dts changes for the ICS-43432 chip ?

I would like to interface this chip to i.MX6.

Thanks for the help.

0 Kudos
984 Views
shabeerbadarudh
Contributor IV

Hi Titus,

Sorry for the late response, have you need any help from me?

0 Kudos