AnsweredAssumed Answered

Watchdog restarts even though it is kicked

Question asked by Haris P on Jan 13, 2017
Latest reply on Jul 2, 2018 by Thomas Viard

imx6ul watchdog not stopping

 

Hi all,

 

I am using imx6ul and I am trying to use the watchdog.

 

I have used  in my board's .h file 

 

   #define CONFIG_IMX_WATCHDOG  

 

to enable the watchdog.

 

Then I go to /uboot_folder/drivers/watchdog/imx_watchdog.c  and check what is done:

 

#ifdef CONFIG_IMX_WATCHDOG
void hw_watchdog_reset(void)
{
struct watchdog_regs *wdog = (struct watchdog_regs *)WDOG1_BASE_ADDR;

writew(0x5555, &wdog->wsr);
writew(0xaaaa, &wdog->wsr);
}

void hw_watchdog_init(void)
{
struct watchdog_regs *wdog = (struct watchdog_regs *)WDOG1_BASE_ADDR;
u16 timeout;

/*
* The timer watchdog can be set between
* 0.5 and 128 Seconds. If not defined
* in configuration file, sets 128 Seconds
*/
#ifndef CONFIG_WATCHDOG_TIMEOUT_MSECS
#define CONFIG_WATCHDOG_TIMEOUT_MSECS 128000
#endif
timeout = (CONFIG_WATCHDOG_TIMEOUT_MSECS / 500) - 1;
writew(WCR_WDZST | WCR_WDBG | WCR_WDE | WCR_WDT | WCR_SRS |

SET_WCR_WT(timeout), &wdog->wcr);

hw_watchdog_reset();
}
#endif

 

I then start my board which runs embedded linux, the board actually restarts  after 128 seconds.

 

However, I try to kick the watchdog by using the following script:

 

while [ 1 ] ; do sleep 1; echo x > /dev/watchdog; done

 

I run this script, the watchdog replies 

 

root@ccimx6ulstarter:~# ./script
watchdog watchdog0: watchdog did not stop!
watchdog watchdog0: watchdog did not stop!
......

......

......

watchdog watchdog0: watchdog did not stop!
watchdog watchdog0: watchdog did not stop!

 

U-Boot dub-2015.04-r5.4+ga397dea (Jan 13 2017 - 15:09:55)

CPU: Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 40C
Reset cause: WDOG
I2C: ready
DRAM: 256 MiB

......

......

......

 

So despite the fact that I am kicking the watchdog, the watchdog restarts. 

 

The same happens when I use command

 

watchdog -t 10 /dev/watchdog

 

The only way of making the system work is not using the WCR_WDE flag. When I do this, the watchdog does not start automatically, but I can start it with

echo V > /dev/watchdog

Then the watchdog starts and with my script I can kick it and when the script ends it restarts. However, I want the watchdog to start automatically with WCR_WDE flag.

 

How can I solve this problem?

 

Thanks

Outcomes