Hello Community
There is parameter named powerManagement for GPU driver of i.MX6.
Could you give me a description about the PM function of i.MX6 GPU?
And in the GPU driver gc_hal_kernel_probe.c(linux-imx-4.1.15/drivers/mxc/gpu-viv/hal/os/linux/kernel)),
the default value for powerManagement is -1.What does -1 mean. My understand is 0 for disable and 1 for enable.I cannot understand -1.
Thank you!
ZongbiaoLiao
refer to the user guide, PM funtion depends on other options when you want to enable or disable it.
"The GPU profiling mode requires the GPU Power Management (PM) functions to be disabled to get the
precise profiling data. When kernel module “galcore” is inserted with gpuProfiler=1, the PM functions in the driver
are not disabled. The PM functions are disabled when VIV_PROFILE is set to 1, 2, or 3, and the application starts.
The PM functions are enabled when VIV_PROFILE is set to 0, and the application starts again."