Vybrid Reference Manual F-Series: flow controal for the UART-A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid Reference Manual F-Series: flow controal for the UART-A

Jump to solution
880 Views
ms2017
Contributor I

Dear Ladies and Gentleman,  

i am under review of the Vybrid Reference Manual F-Series to activate the flow controal for the UART-A.

In chapter 3.8.4.1 there is mentioned, that all uarts support Hardware flow control (RTS/CTS).

However, I did not find any more explanation how to use that feature?

Is there some documentation about that?

E.g. what are the relevant registers?  

Many thanks

0 Kudos
1 Solution
605 Views
ms2017
Contributor I

So to add some explanation, the vybriddrm.pdf vybrid reference manual, rev 7, 06/2014 contains information in chapter 49.4.1.6 Hardware flow control. 

Inside the vfxxx controller reference manual, rev. 0, 10/2016, i could not find that chapter about hardware flow control. Is it still possible to use the mechanism as mentioned in 49.4.1.6.? 

View solution in original post

2 Replies
605 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please create request :

https://community.nxp.com/docs/DOC-329745 

Regards,

Yuri.

0 Kudos
606 Views
ms2017
Contributor I

So to add some explanation, the vybriddrm.pdf vybrid reference manual, rev 7, 06/2014 contains information in chapter 49.4.1.6 Hardware flow control. 

Inside the vfxxx controller reference manual, rev. 0, 10/2016, i could not find that chapter about hardware flow control. Is it still possible to use the mechanism as mentioned in 49.4.1.6.?