AnsweredAssumed Answered

K82 flash locking

Question asked by Chris Westervelt on Jan 12, 2017
Latest reply on Jan 18, 2017 by Chris Westervelt

I’m full steam ahead using the K82 part for an encryption dongle.  I could use some help figuring something out though.  I need to be able to load keys and certificates on to the part and store them in NAND flash.  I also need to lock the NAND after programming so no one can pull code (or keys etc.) from the SWD.  Will that be a conflict and keep me from being to commit data to the NAND from inside the part with it locked?

Outcomes