Dear team,
I would like to ask about the configuration of PCIe related unused pins of i.MX6SoloX.
(1)
In case of not using PCIe, could you show me how PCIe related pins(PCIE_VP and PCIE_VPTX pins) should be treated?
(2)
Could you show me whether shoot-through-current can be prevented when disabling PCIe_LDOs?
(3)
From ‘Figure 10-12. Supplying i.MX 6SoloX power using integrated PMU’ in i.MX6SX reference manual(IMX6SXRM, Rev.1), my customer understands that PCIE_VPH, PCIE_VP and PCIE_VPTX pins should be connected to GND through capacitor when not used.
But according to its HW Devlopement Guide(IMX6SXHDG, Rev.1), the pins should be treated when not used as below.
- PCIE_VPH should be float or connected to ground directly when unused.
- PCIE_VP and PCIE_VPTX pins should be connected to GND through 4.7uF capacitors.
Could you show me which handling is the correct?
Thanks,
Miyamoto
Hi Miyamoto
1.3. in case of not using PCIe please follow recommendations
in HW Devlopement Guide(IMX6SXHDG).
2. there are no known issues with "shoot-through-current" when disabling PCIe_LDO.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------