AnsweredAssumed Answered

imx7s fsl-image-mfgtool-initramfs not complete

Question asked by Edward Tyrrell on Jan 11, 2017

Hello,

 

According to correspondence I have had with fsl community the fsl-image-mfgtool-initramfs is not available for the warp7 board ( imx7s-warp ). If bitbaking fsl-image-mfgtool-initramfs with Krogoth it produces the following error:

 

NOTE: make -j 4 imx7s-warp.dtb
|   CC      scripts/mod/empty.o
|   CC      scripts/mod/devicetable-offsets.s
|   MKELF   scripts/mod/elfconfig.h
|   HOSTCC  scripts/mod/modpost.o
|   HOSTCC  scripts/mod/sumversion.o
|   GEN     scripts/mod/devicetable-offsets.h
|   HOSTCC  scripts/mod/file2alias.o
|   HOSTLD  scripts/mod/modpost
| make[3]: *** No rule to make target `arch/arm/boot/dts/imx7s-warp.dtb'.  Stop.
| make[2]: *** [imx7s-warp.dtb] Error 2
| make[1]: *** [sub-make] Error 2
| make: *** [__sub-make] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/ed/fs-community-bsp-krogoth-imx7sabresd/build-warp7/tmp/work/imx7s_warp-poky-linux-gnueabi/mfgtool-linux-imx/4.1.15-r0/temp/log.do_compile.10292)
ERROR: Task 185 (/home/ed/fs-community-bsp-krogoth-imx7sabresd/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 978 tasks of which 0 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

 

 

The same command for the imx7dsabresd works. So, Has any one updated the recipe for the imx7s-warp or can someone give me some pointers based on the imx7dsabresd how too?

 

BR,

 

Ed.

Outcomes