imx7d android starting not stop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7d android starting not stop

1,072 Views
zhghua1103
Contributor I

Dear All,

Thanks very much about the error:

such as

 

174257_174257.jpg1912593421.jpg

this is my  logcat:

 

root@sabresd_7d:/system/media/audio/alarms # logcat
--------- beginning of main
01-01 00:00:00.440   178   178 W auditd  : type=2000 audit(0.0:1): initialized
01-01 00:00:12.242   188   188 I /system/bin/tzdatacheck: tzdata file /data/misc/zoneinfo/current/tzdata does not exist. No action requi.
01-01 00:00:12.991   192   192 I lowmemorykiller: Using in-kernel low memory killer interface
--------- beginning of system
01-01 00:00:13.051   185   185 I vold    : Vold 3.0 (the awakening) firing up
01-01 00:00:13.051   185   185 V vold    : Detected support for: ext4 f2fs vfat
01-01 00:00:13.059   185   185 W Vold    : Tearing down stale mount /mnt/shm
01-01 00:00:13.091   194   194 I SurfaceFlinger: SurfaceFlinger is starting
01-01 00:00:13.091   194   194 I SurfaceFlinger: SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
01-01 00:00:13.110   194   194 D libEGL  : loaded /system/lib/egl/libGLES_android.so
01-01 00:00:13.197   194   194 I imx7.gralloc: fb_device_open dispid:0, fb:0
01-01 00:00:13.197   194   194 I imx7.gralloc: 16bpp setting of Framebuffer with RGB565 format!
01-01 00:00:13.197   194   194 W imx7.gralloc: using (fd=13)
01-01 00:00:13.197   194   194 W imx7.gralloc: id           = mxc_epdc_fb
01-01 00:00:13.197   194   194 W imx7.gralloc: xres         = 1200 px
01-01 00:00:13.197   194   194 W imx7.gralloc: yres         = 825 px
01-01 00:00:13.197   194   194 W imx7.gralloc: xres_virtual = 1200 px
01-01 00:00:13.197   194   194 W imx7.gralloc: yres_virtual = 2688 px
01-01 00:00:13.197   194   194 W imx7.gralloc: bpp          = 16
01-01 00:00:13.197   194   194 W imx7.gralloc: r            = 11:5
01-01 00:00:13.197   194   194 W imx7.gralloc: g            =  5:6
01-01 00:00:13.197   194   194 W imx7.gralloc: b            =  0:5
01-01 00:00:13.197   194   194 W imx7.gralloc: width        = 191 mm (159.581146 dpi)
01-01 00:00:13.197   194   194 W imx7.gralloc: height       = 131 mm (159.961838 dpi)
01-01 00:00:13.197   194   194 W imx7.gralloc: refresh rate = 85.00 Hz
01-01 00:00:13.206   194   194 E FslHwcomposer: Error! hw_get_module fsl_hwc failed
01-01 00:00:13.206   194   194 E FslHwcomposer: Error! hw_get_module viv_hwc failed
01-01 00:00:13.207   194   194 I FslHwcomposer: open /sys/class/graphics/fb0/fsl_disp_dev_property failed
01-01 00:00:13.207   194   194 W FslHwcomposer: system can't support more than 1 devices
01-01 00:00:13.207   194   194 W FslHwcomposer: invalid refresh rate, assuming 60 Hz
01-01 00:00:13.207   194   194 I FslHwcomposer: hwcomposer: open framebuffer fb0
01-01 00:00:13.207   194   194 I imx7.gralloc: fb_device_open dispid:0, fb:0
01-01 00:00:13.207   194   194 I imx7.gralloc: display already initialized...
01-01 00:00:13.207   194   194 I FslHwcomposer: hwc_device_open,426
01-01 00:00:13.207   194   194 I SurfaceFlinger: Using composer version 1.3
01-01 00:00:13.207   194   194 E FslHwcomposer: unknown display attribute 6
01-01 00:00:13.207   194   194 W SurfaceFlinger: no suitable EGLConfig found, trying a simpler query
01-01 00:00:13.207   194   194 W SurfaceFlinger: EGL_SLOW_CONFIG selected!
01-01 00:00:13.207   194   194 I SurfaceFlinger: EGL information:
01-01 00:00:13.207   194   194 I SurfaceFlinger: vendor    : Android
01-01 00:00:13.207   194   194 I SurfaceFlinger: version   : 1.4 Android META-EGL
01-01 00:00:13.207   194   194 I SurfaceFlinger: extensions: EGL_KHR_get_all_proc_addresses EGL_ANDROID_presentation_time EGL_KHR_swap_b
01-01 00:00:13.207   194   194 I SurfaceFlinger: Client API: OpenGL_ES
01-01 00:00:13.208   194   194 I SurfaceFlinger: EGLSurface: 5-6-5-0, config=0x0
01-01 00:00:13.208   194   194 W SurfaceFlinger: no suitable EGLConfig found, trying a simpler query
01-01 00:00:13.208   194   194 W SurfaceFlinger: EGL_SLOW_CONFIG selected!
01-01 00:00:13.208   194   194 I SurfaceFlinger: EGL information:
01-01 00:00:13.208   194   194 I SurfaceFlinger: vendor    : Android
01-01 00:00:13.208   194   194 I SurfaceFlinger: version   : 1.4 Android META-EGL
01-01 00:00:13.208   194   194 I SurfaceFlinger: extensions: EGL_KHR_get_all_proc_addresses EGL_ANDROID_presentation_time EGL_KHR_swap_b
01-01 00:00:13.208   194   194 I SurfaceFlinger: Client API: OpenGL_ES
01-01 00:00:13.208   194   194 I SurfaceFlinger: EGLSurface: 5-6-5-0, config=0x0
01-01 00:00:13.208   194   194 I SurfaceFlinger: OpenGL ES informations:
01-01 00:00:13.208   194   194 I SurfaceFlinger: vendor    : Android
01-01 00:00:13.208   194   194 I SurfaceFlinger: renderer  : Android PixelFlinger 1.4
01-01 00:00:13.208   194   194 I SurfaceFlinger: version   : OpenGL ES-CM 1.0
01-01 00:00:13.208   194   194 I SurfaceFlinger: extensions: GL_EXT_debug_marker GL_OES_byte_coordinates GL_OES_fixed_point GL_OES_singl
01-01 00:00:13.208   194   194 I SurfaceFlinger: GL_MAX_TEXTURE_SIZE = 4096         
01-01 00:00:13.208   194   194 I SurfaceFlinger: GL_MAX_VIEWPORT_DIMS = 4096        
01-01 00:00:13.209   194   194 E cutils-trace: Error opening trace file: Permission denied (13)
01-01 00:00:13.209   194   194 W SurfaceFlinger: no suitable EGLConfig found, trying a simpler query
01-01 00:00:13.209   194   194 W SurfaceFlinger: EGL_SLOW_CONFIG selected!
01-01 00:00:13.209   194   194 I SurfaceFlinger: EGL information:
01-01 00:00:13.209   194   194 I SurfaceFlinger: vendor    : Android
01-01 00:00:13.209   194   194 I SurfaceFlinger: version   : 1.4 Android META-EGL
01-01 00:00:13.209   194   194 I SurfaceFlinger: extensions: EGL_KHR_get_all_proc_addresses EGL_ANDROID_presentation_time EGL_KHR_swap_b
01-01 00:00:13.209   194   194 I SurfaceFlinger: Client API: OpenGL_ES
01-01 00:00:13.209   194   194 I SurfaceFlinger: EGLSurface: 5-6-5-0, config=0x0
01-01 00:00:13.216   194   194 D SurfaceFlinger: Set power mode=2, type=0 flinger=0xb6b24000
01-01 00:00:13.620   210   212 D libEGL  : loaded /system/lib/egl/libGLES_android.so
01-01 00:00:13.699   210   212 E cutils-trace: Error opening trace file: Permission denied (13)
01-01 00:00:13.768   210   212 I ARMAssembler: generated scanline__00000077:03010102_00000A01_00000000 [  9 ipp] (30 ins) at [0xb54f11f0s
01-01 00:00:13.770   210   212 I ARMAssembler: generated scanline__00000077:03545402_00000A01_00000000 [ 31 ipp] (52 ins) at [0xb54f1270s

 

Would you please help  me?

 

With Best Regards

Joshua

Original Attachment has been moved to: logcat.zip

Labels (1)
Tags (1)
0 Kudos
2 Replies

683 Views
zhghua1103
Contributor I

Dear Igor,

I want to set the env for imx7d-epdc,

Would you please help me about the question?

With Best Regards

Joshua

0 Kudos

683 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zhu

please check memory with ddr test

https://community.freescale.com/docs/DOC-105652 

then rebuild Android uboot and Mfg Tools firmware with new ddr

settings, obtained from ddr test. Use for programming Mfg Tools script

mfgtool2-android-mx7d-sabresd-sd.vbs

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos