Hi,
currently I use the LPC1756 with USB and CAN to send and receive data to a Windows application. For this purpose, an very reliable driver solution exists and a bootloader enables encrypted firmware updates using nice windows applications.
I want to reuse as many as possible existing source.
For a new project, the microcontroller must be automotive specified, have 4 CAN units and best a LQFP48-80 case. Unfortunately I cannot find a matching microcontroller with additional USB.
Of course a small LPC or FTDI could be added or CAN used for firmware updates, but I would like to omit unnecessary complexity. Customers should be able to do configuration or updates directly using a PC or laptop.
Ideas or tips which microcontroller to use are welcome.
Best, Rainer
Hi,
has there been any news in the meantime? The requirement for a current project would be:
- CAN-FD support
- USB
- ARM-Cortex
- LQFP 48-100
- Flash size 128kB+
How can I select in the NXP product selector CAN-FD, there is no option? Or did I oversee something?
Thanks + best regards, Rainer
Hi Rainer
I did a quick check and I believe that we do not have a MCU with all the features that you request on the same chip.
we will launch the S32K that will have up to 6 CAN but this device do not have USB module, maybe you can use a UART instead of the USB adding a USB to serial.
32-bit Automotive General Purpose MCUs|NXP
Regards
Vicente Gomez