LS1043A Real Time Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A Real Time Application

951 Views
byengsunyang
Contributor II

Hello,

I would like to use Software Real Time Linux with the LS1043A. The LS1043A is not mentioned in hardware that supports PREEMPT_RT in Section 8.4.1 of the SDK 2.0 document.
Does it mean i can not use this feature even if i enable RT in the kernel config or something else ?

Labels (1)
2 Replies

805 Views
Pavel
NXP Employee
NXP Employee

Realtime support is not available in SDK 2.0-1611 as 4.1.30 is not the official version supported by Realtime kernel.

See the Table 13 of the QorIQ SDK 2.0-1611 Documentation:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

805 Views
byengsunyang
Contributor II

Thank you!

If I patched the rt version of the kernel, is that functionality available? In this case, I wonder if the SDK will build stable builds.

0 Kudos