i am using the i.MX 6QuadPlus/6Quad/6DualLite SABREAI Platform 4.1 Board hardware with HDMI display,nothing displayed in hdmi display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i am using the i.MX 6QuadPlus/6Quad/6DualLite SABREAI Platform 4.1 Board hardware with HDMI display,nothing displayed in hdmi display

1,082 Views
maduravula
Contributor II

i am using the i.MX 6QuadPlus/6Quad/6DualLite SABREAI
Platform with the HDMI display.when i connected the board with the hdmi display,the hdmi screen blink and it coming to normal state when it is powered on. i am newbie to this platform,pls give some advice.
 

log message :

U-Boot 2015.04-00392-g6581aea-dirty (Jul 02 2016 - 14:05:01)

CPU: Freescale i.MX6Q rev1.2 at 792 MHz

CPU: Temperature 35 C

Reset cause: POR

Board: MX6Q-Sabreauto revA

I2C: ready

DRAM: 2 GiB

PMIC: PFUZE100 ID=0x10

NAND: 0 MiB

MMC: FSL_SDHC: 0, FSL_SDHC: 1

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In: serial

Out: serial

Err: serial

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:1

Net: FEC [PRIME]

Normal Boot

Hit any key to stop autoboot: 0

boota mmc1

fkernel @ 14008000 (8723472)

ramdisk @ 15000000 (1027930)

fdt @ 14f00000 (47398)

## Booting Android Image at 0x12000000 ...

Kernel load addr 0x14008000 size 8520 KiB

Kernel command line: console=ttymxc3,115200 androidboot.console=ttymxc3 consoleblank=0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1280x800M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=320M

## Flattened Device Tree blob at 14f00000

Booting using the fdt blob at 0x14f00000

Loading Kernel Image ... OK

Using Device Tree in place at 14f00000, end 14f0e925

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 4.1.15-03565-g9f38c97-dirty (b14301@scmbld4) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #1 SMP PREEMPT Fri Jul 1 17:39:29 CST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Freescale i.MX6 Quad SABRE Automotive Board

cma: Reserved 320 MiB at 0x3c000000

Memory policy: Data cache writealloc

PERCPU: Embedded 13 pages/cpu @e4f9a000 s22144 r8192 d22912 u53248

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 522816

Kernel command line: console=ttymxc3,115200 androidboot.console=ttymxc3 consoleblank=0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1280x800M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=320M androidboot.serialno=0e0c79d4e6b34649

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1731796K/2096128K available (11566K kernel code, 972K rwdata, 3688K rodata, 1024K init, 654K bss, 36652K reserved, 327680K cma-reserved, 1145856K highmem)

Virtual kernel memory layout:

vector : 0xffff0000 - 0xffff1000 ( 4 kB)

fixmap : 0xffc00000 - 0xfff00000 (3072 kB)

vmalloc : 0xe6800000 - 0xff000000 ( 392 MB)

lowmem : 0xc0000000 - 0xe6000000 ( 608 MB)

pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)

modules : 0xbf000000 - 0xbfe00000 ( 14 MB)

.text : 0xc0008000 - 0xc0fe5a34 (16247 kB)

.init : 0xc1000000 - 0xc1100000 (1024 kB)

.data : 0xc1100000 - 0xc11f33d0 ( 973 kB)

.bss : 0xc11f33d0 - 0xc1296f64 ( 655 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

Additional per-CPU info printed with stalls.

NR_IRQS:16 nr_irqs:16 16

L2C-310 erratum 769419 enabled

L2C-310 enabling early BRESP for Cortex-A9

L2C-310 full line of zeros enabled for Cortex-A9

L2C-310 ID prefetch enabled, offset 16 lines

L2C-310 dynamic clock gating enabled, standby mode enabled

L2C-310 cache controller enabled, 16 ways, 1024 kB

L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001

mxc_clocksource_init 3000000

Switching to timer-based delay loop, resolution 333ns

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns

clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux: Initializing.

AppArmor: AppArmor disabled by boot time parameter

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

Initializing cgroup subsys freezer

Initializing cgroup subsys debug

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x10100000 - 0x10100058

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (24.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

CPU identified as i.MX6Q, silicon rev 1.2

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

VDSO is not a valid ELF object!

imx6q-pinctrl 20e0000.iomuxc: no groups defined in /soc/aips-bus@02000000/iomuxc@020e0000/hdmicecgrp

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!

mxs-dma 110000.dma-apbh: initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator

2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA

i2c i2c-2: IMX I2C adapter registered

i2c i2c-2: can't use DMA

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.20

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

Switched to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 1004K (c5000000 - c50fb000)

CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]

hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

imx rpmsg driver is registered.

Bus freq driver module loaded

console [pstore-1] enabled

pstore: Registered ramoops as persistent store backend

ramoops: attached 0x100000@0x8bf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink subsys (disabled)

audit: type=2000 audit(0.470:1): initialized

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

ntfs: driver 2.1.32 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.23)

bounce: pool size: 64 pages

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

pwm-backlight supply power not found, using dummy regulator

MIPI DSI driver module loaded

MIPI DSI driver module loaded

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1280x800@60: CVT Name - 1.024MA

mxc_sdc_fb fb@0: registered mxc display driver hdmi

imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 160x45

mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!

mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!

mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: no event needs to be remapped

imx-sdma 20ec000.sdma: loaded firmware 3.3

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

pfuze100-regulator 1-0008: pfuze100 found.

mxc_hdmi 20e0000.hdmi_video: Read EDID again

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 298, base_baud = 5000000) is a IMX

21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 299, base_baud = 5000000) is a IMX

mxc_hdmi 20e0000.hdmi_video: create default modelist

console [ttymxc3] enabled

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

zram: Created 1 device(s)

si476x-core 1-0063: Using default platform data.

si476x-core 1-0063: No IRQ number specified, will use polling

si476x-core 1-0063: Error while sending command 0x11

si476x-core 1-0063: The device in inconsistent power state

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

2188000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver

usbcore: registered new interface driver pegasus

usbcore: registered new interface driver rtl8150

usbcore: registered new interface driver r8152

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver cdc_eem

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver usbserial_generic

usbserial: USB Serial support registered for generic

usbcore: registered new interface driver ftdi_sio

usbserial: USB Serial support registered for FTDI USB Serial Device

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

usbcore: registered new interface driver usb_ehset_test

2184800.usbmisc supply vbus-wakeup not found, using dummy regulator

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

egalax_ts 1-0004: Failed to wake up, disable suspend,otherwise it can not wake up

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

2-0044 supply vdd not found, using dummy regulator

input: isl29023 light sensor as /devices/virtual/input/input1

isl29023 2-0044: driver version 1.0 enabled

snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x/sz) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR SANYO protocol handler initialized

IR Sharp protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

IR XMP protocol handler initialized

DBG sensor data is at c126e068

mxc_v4l2_output v4l2_out: V4L2 device registered as video16

mxc_v4l2_output v4l2_out: V4L2 device registered as video17

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

2-000e supply vdd not found, using dummy regulator

2-000e supply vddio not found, using dummy regulator

mag3110 2-000e: check mag3110 chip ID

input: FreescaleMagnetometer as /devices/virtual/input/input2

input: eCompass as /devices/virtual/input/input3

mag3110 2-000e: mag3110 is probed

2-001c supply vdd not found, using dummy regulator

2-001c supply vddio not found, using dummy regulator

input: FreescaleAccelerometer as /devices/virtual/input/input4

mma8x5x device driver probe successfully

imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.31.0-ioctl (2015-3-12) initialised: dm-devel@redhat.com

Bluetooth: HCI UART driver ver 2.3

Bluetooth: HCI UART protocol H4 registered

Bluetooth: HCI UART protocol BCSP registered

Bluetooth: HCI UART protocol ATH3K registered

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified

sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified

sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO

sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

218c000.mlb supply reg_nvcc not found, using dummy regulator

mxc_mlb150 218c000.mlb: enalbe regulator

mxc_vpu 2040000.vpu_fsl: VPU initialized

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

imx6q-pinctrl 20e0000.iomuxc: unable to find group for node hdmicecgrp

imx6q-pinctrl 20e0000.iomuxc: unable to find group for node hdmicecgrp

mxc_hdmi_cec soc:hdmi_cec@00120000: can't get/select CEC pinctrl

Galcore version 5.0.11.41671

mmc2: new ultra high speed SDR104 SDHC card at address aaaa

mmcblk2: mmc2:aaaa SE16G 14.8 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

caam 2100000.caam: Entropy delay = 3200

caam 2100000.caam: Instantiated RNG4 SH0

caam 2100000.caam: Instantiated RNG4 SH1

caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)

caam 2100000.caam: job rings = 2, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 2101000.jr0: registering rng-caam

platform caam_sm: blkkey_ex: 4 keystore units available

platform caam_sm: 64-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: 64-bit black key:

platform caam_sm: [0000] c8 f8 e3 37 62 b1 c5 33

platform caam_sm: [0008] 2f d7 70 7c fa d8 91 6f

platform caam_sm: 128-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: 128-bit black key:

platform caam_sm: [0000] d7 0e 73 52 51 5b 8d 7c

platform caam_sm: [0008] c6 73 59 53 ff 51 28 8c

platform caam_sm: 192-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: 192-bit black key:

platform caam_sm: [0000] ae a8 78 e8 5b 88 98 81

platform caam_sm: [0008] 35 c3 f6 3e de 95 63 6c

platform caam_sm: [0016] 4a c7 da fe 22 ee e4 e0

platform caam_sm: [0024] 19 29 fb 76 49 a6 dc c3

platform caam_sm: 256-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f

platform caam_sm: 256-bit black key:

platform caam_sm: [0000] fd 48 c7 da 73 38 13 3e

platform caam_sm: [0008] 4d 80 c1 4c 46 bc 21 f8

platform caam_sm: [0016] 76 15 40 38 c6 b9 03 23

platform caam_sm: [0024] 44 44 e0 0d 1e c1 d7 2d

platform caam_sm: 64-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 196-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 64-bit black key in blob:

platform caam_sm: [0000] 05 6f 95 f7 6f 35 a0 fe

platform caam_sm: [0008] ec b3 20 21 3a 07 e2 75

platform caam_sm: [0016] ab dd 09 a2 fb 36 2e 3f

platform caam_sm: [0024] ad cc ec 93 f1 07 84 02

platform caam_sm: [0032] 05 96 f6 27 a0 88 77 6b

platform caam_sm: [0040] df 23 9d 99 51 5e 7e 89

platform caam_sm: [0048] 25 59 3c 26 d9 dd 14 5a

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit black key in blob:

platform caam_sm: [0000] 2e fa 14 73 bd 12 ae 02

platform caam_sm: [0008] 87 07 b5 cc a7 39 1f 04

platform caam_sm: [0016] ba 74 b9 db 96 d9 f1 9b

platform caam_sm: [0024] 06 cd f1 50 ea 0c 55 83

platform caam_sm: [0032] 1f 81 62 12 86 03 6a fc

platform caam_sm: [0040] 27 43 0d 10 27 c5 0a ed

platform caam_sm: [0048] d5 45 ea 76 9b d8 a4 a3

platform caam_sm: [0056] 69 9b e8 0b 3d 02 72 43

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 192-bit black key in blob:

platform caam_sm: [0000] 17 a8 20 3e bc 16 f2 b9

platform caam_sm: [0008] 7d 57 23 53 b0 fb 8d e1

platform caam_sm: [0016] 6e 98 aa 4a 1a a1 90 ef

platform caam_sm: [0024] 73 5e 8e 22 45 ea 31 54

platform caam_sm: [0032] 76 c4 c2 41 7f 58 31 d3

platform caam_sm: [0040] 88 39 d6 1a 27 be 05 0e

platform caam_sm: [0048] 47 81 10 aa 30 be dd 21

platform caam_sm: [0056] 4c 1a b8 01 cc 8b 93 5f

platform caam_sm: [0064] 31 4d b1 27 28 bc 40 1f

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit black key in blob:

platform caam_sm: [0000] 83 1b 88 03 b9 e5 3b 70

platform caam_sm: [0008] ab 18 d5 52 ce fd 6d 2d

platform caam_sm: [0016] b5 0d 8d 3a fb ce 58 2b

platform caam_sm: [0024] 10 bc 0c 3e ea 51 d6 d5

platform caam_sm: [0032] b3 99 b1 f2 ae d2 08 92

platform caam_sm: [0040] 39 79 b4 bf 33 f0 49 ee

platform caam_sm: [0048] d3 95 b9 3f 53 16 9c 83

platform caam_sm: [0056] db b8 1f 16 1b 50 c4 8a

platform caam_sm: [0064] 59 6d c7 5c f2 96 82 af

platform caam_sm: [0072] 83 f8 0e a0 e4 ae 2d d2

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: restored 64-bit black key:

platform caam_sm: [0000] bc 08 31 b3 9b 5f e9 01

platform caam_sm: [0008] 95 fb bb e0 73 86 f3 45

platform caam_sm: restored 128-bit black key:

platform caam_sm: [0000] d7 0e 73 52 51 5b 8d 7c

platform caam_sm: [0008] c6 73 59 53 ff 51 28 8c

platform caam_sm: restored 192-bit black key:

platform caam_sm: [0000] ae a8 78 e8 5b 88 98 81

platform caam_sm: [0008] 35 c3 f6 3e de 95 63 6c

platform caam_sm: [0016] 5a b7 28 ad 04 4b 0f de

platform caam_sm: [0024] a7 90 af fd 3e 83 ed 1b

platform caam_sm: restored 256-bit black key:

platform caam_sm: [0000] fd 48 c7 da 73 38 13 3e

platform caam_sm: [0008] 4d 80 c1 4c 46 bc 21 f8

platform caam_sm: [0016] 76 15 40 38 c6 b9 03 23

platform caam_sm: [0024] 44 44 e0 0d 1e c1 d7 2d

snvs-secvio 20cc000.caam-snvs: can't get snvs clock

snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

usbcore: registered new interface driver snd-usb-audio

cs42xx8 1-0048: found device, revision 4

fsl-asrc 2034000.asrc: driver registered

imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok

imx-cs42888 sound-cs42888: snd-soc-dummy-dai <-> 2034000.asrc mapping ok

imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok

imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok

imx-tuner-si476x sound-fm: failed to find FM platform device

imx-tuner-si476x: probe of sound-fm failed with error -22

imx-audio-hdmi sound-hdmi: hdmi-hifi <-> soc:hdmi_audio@00120000 mapping ok

NET: Registered protocol family 26

u32 classifier

Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (16384 buckets, 65536 max)

ctnetlink v0.93: registering with nfnetlink.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

can-stby: supplied by can-en

flexcan 2094000.flexcan: device registered (reg_base=ef578000, irq=31)

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 4.1.15-03565-g9f38c97-dirty ehci_hcd

usb usb1: SerialNumber: ci_hdrc.1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

dhd_module_init in

input: gpio-keys as /devices/soc0/gpio-keys/input/input5

snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)

can-stby: disabling

can-en: disabling

usb_otg_vbus: disabling

VGEN2: disabling

SW4: disabling

ALSA device list:

#0: cs42888-audio

#1: imx-spdif

#2: imx-hdmi-soc

Freeing unused kernel memory: 1024K (c1000000 - c1100000)

init: init started!

SELinux: Android master kernel running Android M policy in compatibility mode.

SELinux: Permission audit_read in class capability2 not defined in policy.

SELinux: the above unknown classes and permissions will be denied

audit: type=1403 audit(2.620:2): policy loaded auid=4294967295 ses=4294967295

audit: type=1404 audit(2.630:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: (Initializing SELinux enforcing took 0.15s.)

init: init second stage started!

init: waitpid failed: No child processes

init: property_set("ro.zygote", "zygote32") failed

init: (Loading properties from /default.prop took 0.00s.)

init: (Parsing /init.environ.rc took 0.00s.)

init: (Parsing /init.usb.rc took 0.00s.)

init: (Parsing init.freescale.usb.rc took 0.00s.)

init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)

init: (Parsing /init.freescale.rc took 0.01s.)

init: (Parsing /init.usb.configfs.rc took 0.00s.)

init: (Parsing /init.zygote32.rc took 0.00s.)

init: (Parsing /init.trace.rc took 0.00s.)

init: (Parsing /init.rc took 0.04s.)

init: SELinux: Could not get canonical path /adb_keys restorecon: No such file or directory.

init: Starting service 'ueventd'...

audit: type=1400 audit(2.820:4): avc: denied { mounton } for pid=1 comm="init" path="/sys/kernel/debug" dev="debugfs" ino=1 scontext=u:r:init:s0 tcontext=u:object_r:debugfs:s0 tclass=dir permissive=0

ueventd: ueventd started!

init: Waiting for /dev/.coldboot_done...

ueventd: Coldboot took 0.27s.

init: Waiting for /dev/.coldboot_done took 0.26s.

init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory

init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument

init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory

init: Starting service 'watchdogd'...

Console: switching to colour dummy device 80x30

watchdogd: watchdogd started (interval 10, margin 20)!

fs_mgr: Enabling dm-verity for system (mode 0)

EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: barrier=1

fs_mgr: __mount(source=/dev/block/dm-0,target=/system,type=ext4)=0

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p4): recovery complete

EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p6): recovery complete

EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0

file system registered

init: Starting service 'logd'...

zram0: detected capacity change from 0 to 314572800

audit: type=1400 audit(3.620:5): avc: denied { read write } for pid=200 comm="mkswap" name="zram0" dev="tmpfs" ino=8474 scontext=u:r:toolbox:s0 tcontext=u:object_r:block_device:s0 tclass=blk_file permissive=0

logd.auditd: start

logd.klogd: 5408878333

Unable to find swap-space signature

fs_mgr: swapon failed for /dev/block/zram0

init: (Loading properties from /system/build.prop took 0.01s.)

init: (Loading properties from /vendor/build.prop took 0.00s.)

init: (Loading properties from /factory/factory.prop took 0.00s.)

init: Starting service 'vold'...

init: Not bootcharting.

init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...

init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 209) exited with status 0

random: init urandom read with 31 bits of entropy available

init: Starting service 'logd-reinit'...

init: Starting service 'healthd'...

init: Starting service 'console'...

▒(▒▒init: Starting service 'lmkd'...

init: Starting service 'servicemanager'...

init: Starting service 'surfaceflinger'...

init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No such file or directory

logd.daemon: reinit

init: write_file: Unable to open '/sys/block/mmcblk1/queue/read_ahead_kb': No such file or directory

type=1400 audit(3.890:6): avc: denied { dac_override } for pid=212 comm="sh" capability=1 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

init: Service 'logd-reinit' (pid 210) exited with status 0

root@sabreauto_6q:/ # init: write_file: Unable to open '/sys/class/rfkill/rfkill0/state': No such file or directory

init: property_set("ro.ril.wake_lock_timeout", "300") failed

init: Starting service 'netd'...

init: Starting service 'debuggerd'...

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

init: Starting service 'drm'...

init: Starting service 'media'...

init: Starting service 'installd'...

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

init: Starting service 'keystore'...

init: Starting service 'ril-daemon'...

init: Starting service 'zygote'...

init: Starting service 'gatekeeperd'...

init: cannot find '/system/xbin/perfprofd', disabling 'perfprofd'

init: Starting service 'magd'...

type=1400 audit(4.060:7): avc: denied { unlink } for pid=219 comm="netd" name="netd_pid" dev="mmcblk2p4" ino=817629 scontext=u:r:netd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

android_work: sent uevent USB_STATE=CONNECTED

configfs-gadget gadget: high-speed config #1: b

android_work: sent uevent USB_STATE=CONFIGURED

healthd: No charger supplies found

healthd: No battery devices found

init: Starting service 'bootanim'...

ERROR: unrecognized std! ffffff (PAL=ff, NTSC=b000

capability: warning: `main' uses 32-bit capabilities (legacy support in use)

zram: 510 (system_server) Attribute mem_used_total (and others) will be removed. See zram documentation.

type=1400 audit(12.250:8): avc: denied { unlink } for pid=531 comm="android.bg" name="batterystats.bin" dev="mmcblk2p4" ino=498801 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(12.700:9): avc: denied { unlink } for pid=510 comm="system_server" name="userlist.xml.bak" dev="mmcblk2p4" ino=498800 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

random: nonblocking pool is initialized

type=1400 audit(16.730:10): avc: denied { unlink } for pid=510 comm="system_server" name="packages-backup.xml" dev="mmcblk2p4" ino=498747 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(16.750:11): avc: denied { unlink } for pid=510 comm="system_server" name="packages.list" dev="mmcblk2p4" ino=498793 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(16.760:12): avc: denied { unlink } for pid=510 comm="system_server" name="package-restrictions-backup.xml" dev="mmcblk2p4" ino=498771 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

period -1024674229 ,timeout is -1024639870, wake up is :0

period -1024674229 ,timeout is -1024639870, wake up is :0

type=1400 audit(17.020:13): avc: denied { unlink } for pid=531 comm="android.bg" name="runtime-permissions.xml.bak" dev="mmcblk2p4" ino=498756 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.300:14): avc: denied { unlink } for pid=531 comm="android.bg" name="accounts.xml.bak" dev="mmcblk2p4" ino=498741 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.320:15): avc: denied { unlink } for pid=531 comm="android.bg" name="status.bin.bak" dev="mmcblk2p4" ino=498746 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.340:16): avc: denied { unlink } for pid=531 comm="android.bg" name="stats.bin.bak" dev="mmcblk2p4" ino=498780 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

type=1400 audit(17.670:17): avc: denied { unlink } for pid=552 comm="MountService" name="packages-backup.xml" dev="mmcblk2p4" ino=498747 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.690:18): avc: denied { unlink } for pid=552 comm="MountService" name="packages.list" dev="mmcblk2p4" ino=498793 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.700:19): avc: denied { unlink } for pid=552 comm="MountService" name="package-restrictions-backup.xml" dev="mmcblk2p4" ino=498771 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(17.950:20): avc: denied { unlink } for pid=531 comm="android.bg" name="runtime-permissions.xml.bak" dev="mmcblk2p4" ino=498756 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

acc_open

acc_release

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

type=1400 audit(18.860:21): avc: denied { unlink } for pid=510 comm="system_server" name="journal-613400736.tmp" dev="mmcblk2p4" ino=310692 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(19.100:22): avc: denied { unlink } for pid=587 comm="der-armeabi-v7a" name="libwebviewchromium32.relro" dev="mmcblk2p4" ino=817631 scontext=u:r:shared_relro:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(19.550:23): avc: denied { unlink } for pid=587 comm="der-armeabi-v7a" name="libwebviewchromium32.relro" dev="mmcblk2p4" ino=817631 scontext=u:r:shared_relro:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

mtp_open

type=1400 audit(21.820:24): avc: denied { unlink } for pid=524 comm="Binder_2" name="subtypes.xml.bak" dev="mmcblk2p4" ino=498772 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

type=1400 audit(22.380:25): avc: denied { unlink } for pid=510 comm="system_server" name="wallpaper_info.xml" dev="mmcblk2p4" ino=498774 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

period 66 ,timeout is 0, wake up is :0

mma enable setting active

type=1400 audit(23.490:26): avc: denied { unlink } for pid=510 comm="system_server" name="0.xml.bak" dev="mmcblk2p4" ino=498790 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

mma enable setting inactive

period 66 ,timeout is 0, wake up is :0

mma enable setting active

init: Service 'bootanim' (pid 282) exited with status 0

type=1400 audit(25.480:27): avc: denied { rename } for pid=954 comm="droid.deskclock" name="com.android.deskclock_preferences.xml" dev="mmcblk2p4" ino=678796 scontext=u:r:untrusted_app:s0:c512,c768 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

mma enable setting inactive

type=1400 audit(35.110:28): avc: denied { unlink } for pid=531 comm="android.bg" name="screen_on_time.bak" dev="mmcblk2p4" ino=498803 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0

thanks,

jim.

Tags (2)
0 Kudos
1 Reply

520 Views
igorpadykov
NXP Employee
NXP Employee

Hi jim

for hdmi should be used :

video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32

as described in attached sect.6.3.2 Kernel command line

For programming images please use Demo Images

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.0_AND_DEMO_AI_BSP&appType=license&location=... 

and MFG Tools, use mfgtool2-android-mx6q-sabresd-emmc.vbs script

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.0.0_MFG_TOOL&appType=license&location=null&... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos