工 周

申请LPC54608开发板

Discussion created by 工 周 on Jan 5, 2017

从51的P系列实现简单的控制显示,到Cortex-M3 的LPC1765 实现复杂一点的行车记录仪显示控制,LPC11C24 用于CAN BUS  通信采集。LPC1768用于LCD屏(192*64)显示的公交GPS自动报站调度系统。一路走来已使用NXP MCU 12年了。2017年计划采用LPC54608芯片代替LPC1768,显示屏用7寸TFT_LCD(800*480)屏代替黑白LCD屏用于GUI显示界面,以及增加电阻触摸屏,使用户体验更加视觉完美,操作直观。同时需要6路的UART(4路RS232,2路RS485),及2路CAN(仪表盘CAN数据采集用于后台分析),USB(升级,行车数据导出),SDCARD(报站文件系统存取),以及洛干个GPIO输入传感器信号采集。本项所需求之功能都基本都与LPC54608的资源非常嵌合,有用于公司长期采用,延续采用高稳的NXP MCU系列产品。至此,尽快上手一块LPC54608平估板用于尽快熟悉开发环境及软硬件资源,以及为实际项目有设计软件及硬件做项目前的必要评估都具有极大的价值。能争取不少时间,缩短项目的开发进度。

Outcomes