AnsweredAssumed Answered

Are the Fault polarity must be logic 1 in mc56f8013?

Question asked by Yongsheng Wang on Jan 6, 2017
Latest reply on Jan 8, 2017 by xiangjun.rong

Dear all,

I am using the fault protection of 8013, the Manual book writes" Faults are generated by either a Logic 1 or Logic 0, determined by the fault polarity control bits in the fault control (FCTRL) register on any of the FAULT pins. " However I can't find control bit in the FCTRL. I wonder that if the 8013 support different logic level,especially the logic 0? Thanks a lot!

Outcomes