imx6ulevk uboot启动设置问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ulevk uboot启动设置问题

2,870 Views
xinjianlu
Contributor II

imx6ulevk qspi nor里u-boot header,u-boot.imx 是烧写qspi哪个空间里,换成nand flash芯片烧写是否一样,nfs挂载时,u-boot下如何设置?我用core-image-minimal版本,两个以太网配置不起作用,不能ping通。

Labels (1)
0 Kudos
2 Replies

1,231 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Xinjian,

>>烧写问题

I.MX6UL可以从QSPI端口,NAND端口,SD卡端口启动,这就是说,你可以把U-BOOT烧写在QSPI,NAND, SD卡里都可以。启动时,配置拨码开关选择从哪个端口启动。也就是烧写到哪里,就从哪里启动。

>>NFS启动的问题

我提供一个使用静态IP,从NFS启动android文件系统的U-BOOT环境变量配置,你稍微修改一下,就能启动linux文件系统。在使用NFS之前,你要在你的linux PC主机上做好相应软件包的安装:比如tftp server(通过网络下载内核到板子)、nfs server。参考下面的过程:

1. Setup tftp server
The purpose to configure tftp server is to download the linux kernel from ubuntu host through ethernet to target board.The following
is steps to configure tftp sever:
(1) Setup tftp server files
#sudo apt-get install tftpd tftp openbsd-inetd
(2) make a tftp directory
Here we make /opt/tftpboot be a tftp directory.
# mkdir /opt/tftpboot
# chmod 777 /opt/tftpboot
(3) Open /etc/inetd.conf and edit it
# sudo gedit /etc/inetd.conf
Coment this line :
#tftp dgram udp wait nobody /usr/sbin/tcpd /usr/sbin/in.tftpd /srv/tftp
Add new line:
tftp dgram udp wait nobody /usr/sbin/tcpd /usr/sbin/in.tftpd /opt/tftpboot
(4)Restarting tftp service
#sudo /etc/init.d/openbsd-inetd restart
(5)Restart system
(6)Test tftp service
# cd /opt/tftpboot
# touch test.txt
# cd ~/
# tftp 192.168.1.130
Tftp> get test.txt
If promt:
¡°Received xx bytes in xx seconds ¡°
Then tftp service is working.

2. Setup NFS server
(1) Install NFS server package
#sudo apt-get install nfs-kernel-server
(2) Create NFS directory:/opt/nfsroot
# mkdir /opt/nfsroot
(3) Configure mounted directory and authority
# sudo gedit /etc/exports
Add the following line at the end of the file:
/opt/nfsroot *(rw,sync,no_root_squash)

pastedImage_1.png

(4) Restart the NFS service
#sudo /etc/init.d/portmap restart
#sudo /etc/init.d/nfs-kernel-server restart
(5)Test NFS server
# sudo mkdir /mnt/nfs-here
# cd /opt/nfsroot
# touch nfstest
# sudo mount -t nfs 192.168.1.6:/opt/nfsroot /mnt/nfs-here/
# cd /mnt/nfs-here
# ls
Then you will find nfstest file is here , It indicates that your
NFS server is correctly working.
Note : If you want to cancel the above mounting , you can use this
command:
# cd /mnt (or cd ../)
# sudo umount /mnt/nfs-here

pastedImage_2.png

NOTE:
To restart network , the following Command can be used :
Restart Network : sudo /etc/init.d/networking restart

3、配置NFS举例:

setenv ipaddr 192.168.1.103
setenv serverip 192.168.1.102
setenv gateway 192.168.1.1
setenv ethaddr 00:04:9f:00:ea:d3
setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
setenv bootargs_android 'setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale'
setenv bootargs_nfs 'setenv bootargs ${bootargs} ip=${ipaddr}:${serverip}:${gateway}:${netmask}::eth0 off root=/dev/nfs nfsroot=${serverip}:${nfsroot}'
setenv bootargs_disp 'setenv bootargs ${bootargs} video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off fbmem=10M
vmalloc=400M'
setenv bootcmd_net 'run bootargs_base bootargs_android bootargs_nfs bootargs_disp;tftpboot ${loadaddr} uImage;bootm'

>>core-image-minimal网络

启动系统后,你可以利用ifconfig或者netcfg看看网络设备情况,如果都没有,说明core-image-minimal中没有包含进去网络驱动。你可以尝试重新加入网络部分,编译好,再试试。

伟东

0 Kudos

1,231 Views
xinjianlu
Contributor II

hi,你好!

在u-boot下通过tftp烧 zImage rootfs.jffs2到qspi里,就是不知道u-boot.imx是烧写qspi哪个地址下,还u-boot 的引导头是烧写到QSPI哪个地址里?

用ifconfig 可以看到列两个设备,但是用ifconfig eth1 可配置成功,另一个不能成功,ping其他设备地址失败。

0 Kudos