关于BGU8051在TDD模式下使用问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于BGU8051在TDD模式下使用问题

888 Views
gyb1986729
Contributor I

大家好!

        BGU8051使用在TDD模式下,如果要实现BGU8051处于常开的状态,引脚6的电压是0V还是2V,或者是用一个矩形方波进行控制,希望有用过此芯片的人给予指点!

0 Kudos
1 Reply

789 Views
andrei_skok
NXP Employee
NXP Employee

"Hello everyone! BGU8051 used in TDD mode, if you want to achieve BGU8051 in a normally open state, pin 6 of the voltage is 0V or 2V, or with a rectangular square wave control, hope that the chip used to give guidance to the people!"

Please look at the Table 8, Shutdown control in the BGU8051 Datasheet http://www.nxp.com/documents/data_sheet/BGU8051.pdf 

On state -   < 0.6V on Pin 6 (SHDN)

Off state -   > 1.2V on Pin 6 (SHDN)

0 Kudos