Hi All,
In one of our project we are using imx6solo and yocto build system(jethro_4.1.15-1.1.0_GA)
We have requirement for HAB4 and downloaded the CST -2.3.2 tool from NXP server.
We are enable the HAB at U-Boot and kernel(/sys/fsl_otp).
Now we write the mw 021bc2460 2 for enable the HAB on engineering mode
When we use the hab_status at U-boot prompt it shows “ Secure boot enabled”
When we trying for hab_auth_image we are getting the following error
Can you please help for fixing this issue .
=> hab_auth_img 0x12000000 0x559000
Authenticate image from DDR location 0x12000000...
ivt_offset = 0x559000, ivt addr = 0x12559000
Dumping IVT
12559000: 402000d1 12001000 00000000 00000000 .. @............
12559010: 00000000 12559000 12559020 00000000 ......U. .U.....
Dumping CSF Header
12559020: 404800d4 000c00be 00001703 48000000 ..H@...........H
12559030: 020c00be 01000009 88040000 000c00ca ................
12559040: 0000c501 dc070000 000c00be 02000009 ................
12559050: e0090000 001400ca 0000c502 340d0000 ...............4
Secure boot enabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x00
0x00 0x00 0x00 0x20
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x20
0x00 0x00 0x00 0x01
--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x80 0x00
0x00 0x00 0x00 0x04
Calling authenticate_image in ROM
ivt_offset = 0x559000
start = 0x12000000
bytes = 0x55b020
Secure boot enabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x00
0x00 0x00 0x00 0x20
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x20
0x00 0x00 0x00 0x01
--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x90 0x80 0x00
0x00 0x00 0x00 0x04
--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x12 0x55 0x90 0x00
0x00 0x00 0x00 0x20
And also pls help for signing the SPL image.
Thanks & Regards
Kilaru Ramakrishna Rao
Original Attachment has been moved to: genIVT.zip
Original Attachment has been moved to: habimagegen.zip
Original Attachment has been moved to: habUImageGen.zip
Original Attachment has been moved to: u-boot.csf.zip
Original Attachment has been moved to: uImage-signed-pad.bin.zip
Original Attachment has been moved to: u-boot-signed-pad.bin.zip
Original Attachment has been moved to: uImage.zip
Original Attachment has been moved to: uImage.csf.zip
Original Attachment has been moved to: u-boot.img.zip
Hello,
Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request.
https://community.nxp.com/docs/DOC-329745
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!