AnsweredAssumed Answered

Camera driver integration on the Sabre Platform (i.MX 6Quad)

Question asked by Bipin Kumar on Jan 3, 2017
Latest reply on Jan 16, 2017 by Yuri Muhin

Actually we want to integrate our 3D camera driver to platform level on the Sabre platform (i.MX 6Quad). I have gone through the source code of the i.MX 6Quad. They have implemented MIPI CSI camera interface for transferring the image the data and the controling of the camera is done by using I2C. But our requirement is to implement the camera by using MIPI CSI for image transfer and controling the camera by using SPI. But i am not able to see the SPI driver on the platform level. 

So my basic query is that "Is it possible to integrate the camera driver with MIPI CSI as transfering the image and SPI for controling the camera on the Platform level".

Outcomes