Hi,
Let me know if you need feedback for this question.
Keep in mind there are restriction with the math library.
Extract of the Targeting_56800E.pdf manual page 81:
This chapter explains considerations for using C with the DSP56800E processor.
Note that the DSP56800E processor does not support:
• The C++ language
• Standard C trigonometric and algebraic floating-point functions (such as sine, cosine, tangent, and square root)
There are some intrinsic functions. Please refer page 198.
And for sure Processor Expert can be used.
Regards
Pascal