The program can't be downloaded or debuged to the KE15Z FRDM.
Here is what I do to the KE15Z FRDM.
1 download the KSDK from kex.nxp.com.
2
download the OpenSDA V2.1 J-link Firmware and put it into the bootloader.
and then link the frdm with the PC via USB cable.
and the the com14 is communication com.
3 open the project by KDS(the latest version),build up the project
click on the debug button,
and then
If you know where i am wrong ,please help me
Hi aline,
Since you have download the OpenSDA V2.1 J-link Firmware, you should select GDB SEGGER J-Link debugger.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------