AnsweredAssumed Answered

BLE Chip requirements...........?

Question asked by muhammed iqbal on Jan 2, 2017

Hai 

i am working with an IOT project . so i would like to know that whether any of your product can QN902x,MKW40Z160 can meet the following requirements..........?

 

 

 

1. is it possible to get the MAC address of a device when it is connected to the ble chip.........?

2. if it is possible to get the MAC can i store the mac in non-volatile memory..............?

3. can i use the chip to transmit some sensor data without connect to it like beacon or broad cast...............?

4.if it is possible to broad cast data can i use a second chip to read this data and perform some actions based on this data.............?

and also 

## what will be the current consumption when it transmit at maximum power and 10sec of TX interval............?

 

 

thank you

Outcomes