network can tftp the boot.img, but when m6.0.1_2.1.0-ga boot up, display error:
fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch
libphy: PHY fixed-0:00 not found
fec 2188000.ethernet eth0: could not attach to PHY
IP-Config: Failed to open eth0
IP-Config: No network devices available
my phy chip is RTL8211FDI, what should i check? thanks.
i enabled VENDOR_REALTEK or REALTEK_PHY in kernel, but there isn't effect.
attached file is my boot info.
Original Attachment has been moved to: minicom1950.cap.zip
in the dtsi file, have you set the phy properly?
e.g. the gpio pin for resetting the phy
i modified the dtsi, add reset delay 100ms,but no effect.
but i add more delay(100ms) after reset in fec_main.c, so it works.
thanks a lot.