AnsweredAssumed Answered

Using battery pack with PF3000 PMIC

Question asked by Johyn Papin on Dec 28, 2016
Latest reply on Jan 10, 2017 by Artur Petukhov

Hello.
I want to know if it is possible to use a Li Ion battery with the PF3000 PMIC.
I actually want that if the module is connected via USB, then the battery is recharged and the module is powered by USB.

Then, I want that if the module is disconnected from the USB, the battery takes over.
This is in fact the same operation as for a smartphone.

Is it possible to carry out such an assembly with the help of PF3000, or is it necessary to add something?

 

Thank you in advance, best regards.

Outcomes