CAAM - SHA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM - SHA

689 Views
jessicapujol
Contributor I

Hello,

I am trying to use the CAAM on iMX6.

Using the supplied SDK, I managed to implement the component and use AES ECB 128 successfully.
Now I have to use the SHA-1 but when I run the job ring, the CAAM hangs on.
The descriptor is as follows:

0xB0800006

0x8441000D

0x24140010

@Pointer to plain text buffer

0x60300010

@pointer to ciphered text buffer

Do you have any idea of the error in my descriptor ?

Thanks

Jessica  

Tags (1)
0 Kudos
2 Replies

449 Views
jessicapujol
Contributor I

Hello Yuri,

Thanks for the link but the guy does not explain which bits were wrong so I do not know if we have the same problem and how he solved it.

Jessica

0 Kudos

449 Views
Yuri
NXP Employee
NXP Employee

Hello

  Please look at https://community.nxp.com/message/654699 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos