AnsweredAssumed Answered

Enabling collaboration on KSDK Device Drivers in github

Question asked by Max Vilimpoc on Dec 26, 2016

Is there any chance NXP would consider allowing for more collaborative development of device drivers and SDK code in github?

 

 

It seems like it would be a benefit to anyone working on Kinetis or LPC devices to have faster access to upstream code changes via a platform like Github, and any helpful modifications would also be easier to pull back in from the community...

 

I mention this because of another question I just asked, in which case it would be pretty easy to create a pull request for changes I could make that would benefit others.

 

One can also see the benefits of this model working for the rapidly-evolving mbed platform.

Outcomes