AnsweredAssumed Answered

Using lauterbach to debug a crashed imx6q (sabresd) board

Question asked by gohilurvish on Dec 26, 2016
Latest reply on Dec 29, 2016 by gohilurvish

Hello Guys,

I'm using a sabresd board which is running linux and on top of that my console based application.

The application crashes at some point.

 

Is it possible to attached lauterbach debugger with trace32 software after the crash is observed? It should not reset the board. Moreover, the debugger was not at all attached when the board was powered on.

 

If this is possible, can someone help me with cmm script to be used for sabresd board (or in last case, imx6 chip)?

 

Thanks,

Urvish.

Outcomes