Hello NXP,
First of all, thank you for your extensive Thread documentation, it is very helpful
I am working on a design using a KW41-based module (Rigado's R41Z) as a black-box Thread modem, which will be controlled by a host via UART. This raises a few questions :
I will also create a small test board with and USB/UART converter to test a minimalist setup. Where can I find some examples of "raw" UART messages that I can send via putty to check if the module is alive?
Thank you for your help.
Best,
Armel
Solved! Go to Solution.
Hi ,
-The example that you want to flash it will depend to the example that you want run.
Please take a look for the documentation, Kinetis Thread Stack Demo Applications User’s Guide.
8 Demo Functionality Overview
C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\Thread
-You can take a look for the next table in the Reference manual.
2.2 Signal Multiplexing and Pin Assignments
-That lines are required if you are using Hardware control.
-Also you can find Low power Uarts Drivers
C:\NXP\MKW41Z_ConnSw_1.0.2\boards\frdmkw41z\driver_examples\lpuart
Hope it helps,
Mario
Hi ,
-The example that you want to flash it will depend to the example that you want run.
Please take a look for the documentation, Kinetis Thread Stack Demo Applications User’s Guide.
8 Demo Functionality Overview
C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\Thread
-You can take a look for the next table in the Reference manual.
2.2 Signal Multiplexing and Pin Assignments
-That lines are required if you are using Hardware control.
-Also you can find Low power Uarts Drivers
C:\NXP\MKW41Z_ConnSw_1.0.2\boards\frdmkw41z\driver_examples\lpuart
Hope it helps,
Mario