PN7462AU VBUS at 3.3V results to Target error from Commit Flash write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462AU VBUS at 3.3V results to Target error from Commit Flash write

Jump to solution
744 Views
stefanmueller
Contributor II

Hi,

we bought the development kit PNEV7462B.

According to user manual UM10883.pdf we used following configuration

- chapter 3.1: External power supply

- chapter 3.2: VBUS set to 3.3V

Now we can't debug the device. We receive following message

15: Target error from Commit Flash write

When I set VBUS to 5V, it debugging is running.

According to manual, the device should run with 3.3V, or?

What else do I have to do?

Thanks and best regards

Stefan

Labels (1)
0 Kudos
1 Solution
477 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Stefan,

    I checked schematic of  PN7462AU EVK board and it's data sheet, in datasheet, there are some description on PVDD, see following,please!

-----------

8.15.2.2 PVDD_LDO

...

   The PVDD_LDO provides 3.3 V supply, that can be used for all digital pads. It may also be used to provide 3.3 V power to external components, avoiding an external LDO. It is supplied by VBUS, and requires a minimum voltage of 4 V to be functional. It delivers a maximum of 30 mA.
   The output pin for PVDD_LDO is PVDD_OUT.
   PVDD_LDO is used to provide the necessary supply to PVDD_IN and PVDD_M_IN (pad supply for master interfaces).
When an external supply is used, PVDD_OUT must be connected to the ground. When
the LDO output is connected to the ground, the PN7462 chip switches off the PVDD_LDO.
...
So JP42 should be connected to GND when using external 3.3V, please try it !
Best Regards,
Weidong

View solution in original post

0 Kudos
2 Replies
478 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Stefan,

    I checked schematic of  PN7462AU EVK board and it's data sheet, in datasheet, there are some description on PVDD, see following,please!

-----------

8.15.2.2 PVDD_LDO

...

   The PVDD_LDO provides 3.3 V supply, that can be used for all digital pads. It may also be used to provide 3.3 V power to external components, avoiding an external LDO. It is supplied by VBUS, and requires a minimum voltage of 4 V to be functional. It delivers a maximum of 30 mA.
   The output pin for PVDD_LDO is PVDD_OUT.
   PVDD_LDO is used to provide the necessary supply to PVDD_IN and PVDD_M_IN (pad supply for master interfaces).
When an external supply is used, PVDD_OUT must be connected to the ground. When
the LDO output is connected to the ground, the PN7462 chip switches off the PVDD_LDO.
...
So JP42 should be connected to GND when using external 3.3V, please try it !
Best Regards,
Weidong
0 Kudos
477 Views
stefanmueller
Contributor II

Dear Weidong,

thank you for your anwer.

I closed JP42 and I replaced

- R179 to R177

- R181 to 180

it works, thank you very much.

Best Regards

Stefan

0 Kudos