AnsweredAssumed Answered

Simultaneous internal and external connection to SCT input?

Question asked by Joseph Dupre on Dec 22, 2016
Latest reply on Jan 3, 2017 by Joseph Dupre

Is it possible to set up an SCT input so that it is connected to an external pin AND the output of another SCT?

 

I have SCT0 set up with one input from an external pin.  The input is normally high, and receives low pulses on occasion.

What I would like to do is:
1. Internally route an output from SCT0 to an SCT1 input.
2. Internally route an output from SCT1 to SCT0's existing external input, so that low pulses can be "injected".

 

It looks like doing (1) is no problem.
But is it possible to have an SCT input connected to both an external pin and another SCT output internally at the same time?  I don't see how to do this, even with the SCTIPU.

 

Thank you,

 

- Joe

Outcomes