We need qual data for part number MPXHZ6115A6T1. We need lifetest data (1000 Hr, 125 C preferred), temp cycling (500 cycles) and HAST or 85/85. Also, what is the terminal finish, ESD rating and MSL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We need qual data for part number MPXHZ6115A6T1. We need lifetest data (1000 Hr, 125 C preferred), temp cycling (500 cycles) and HAST or 85/85. Also, what is the terminal finish, ESD rating and MSL?

588 Views
joseph_barrows
Contributor I

We need lifetest data (1000 Hr, 125 C preferred), temp cycling (500 cycles) and HAST or 85/85. Also, what is the terminal finish, ESD rating and MSL?

0 Kudos
2 Replies

406 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Joseph,

In order to get the requested qual data, please create a standart ticket.

Lead frame base metal is copper. Lead finish is gold over nickel/palladium (NiPdAu).

ESD: ESD (Class 1) - our parts meet the following qualification requirements:

ESD (AEC-Q100) Electrostatic Discharge; Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts

ESD (AEC-Q100) Electrostatic Discharge; Machine Model (MM); Test @ 50/100/150/200 Volts

The MSL rating is blank in the Environmental and Compliance Information section of our web site. The MSL is officially N/A (Not Applicable), since the sensor is open to air (for the pressure to get inside).

Best regards,

Tomas

0 Kudos

406 Views
joseph_barrows
Contributor I

Tomas,

I submitted a standard ticket but received no response and still need qual data.  Thanks for your help thus far, but I still need the qual data.

Thanks,

Joe Barrows

0 Kudos