AnsweredAssumed Answered

fsl-arm-yocto-L4.1.15_2.0.0 problem

Question asked by 贾继中 贾继中 on Dec 22, 2016
Latest reply on Dec 28, 2016 by jimmychan

Ubuntu14.04.05 LTS 64bit

jiajizhong@ubuntu:~$ gcc -v
Using built-in specs.
COLLECT_GCC=gcc
COLLECT_LTO_WRAPPER=/usr/lib/gcc/x86_64-linux-gnu/4.8/lto-wrapper
Target: x86_64-linux-gnu
Configured with: ../src/configure -v --with-pkgversion='Ubuntu 4.8.4-2ubuntu1~14.04.3' --with-bugurl=file:///usr/share/doc/gcc-4.8/README.Bugs --enable-languages=c,c++,java,go,d,fortran,objc,obj-c++ --prefix=/usr --program-suffix=-4.8 --enable-shared --enable-linker-build-id --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --with-gxx-include-dir=/usr/include/c++/4.8 --libdir=/usr/lib --enable-nls --with-sysroot=/ --enable-clocale=gnu --enable-libstdcxx-debug --enable-libstdcxx-time=yes --enable-gnu-unique-object --disable-libmudflap --enable-plugin --with-system-zlib --disable-browser-plugin --enable-java-awt=gtk --enable-gtk-cairo --with-java-home=/usr/lib/jvm/java-1.5.0-gcj-4.8-amd64/jre --enable-java-home --with-jvm-root-dir=/usr/lib/jvm/java-1.5.0-gcj-4.8-amd64 --with-jvm-jar-dir=/usr/lib/jvm-exports/java-1.5.0-gcj-4.8-amd64 --with-arch-directory=amd64 --with-ecj-jar=/usr/share/java/eclipse-ecj.jar --enable-objc-gc --enable-multiarch --disable-werror --with-arch-32=i686 --with-abi=m64 --with-multilib-list=m32,m64,mx32 --with-tune=generic --enable-checking=release --build=x86_64-linux-gnu --host=x86_64-linux-gnu --target=x86_64-linux-gnu
Thread model: posix
gcc version 4.8.4 (Ubuntu 4.8.4-2ubuntu1~14.04.3)

 

 

 

DISTRO=fsl-imx-wayland MACHINE=imx6dlsabresd source fsl-setup-release.sh -b bld-wayland

bitbake fsl-image-qt5

get errors below

 

 

| /bin/bash: line 1: 87203 Killed build/genautomata ../../../../../../../work-shared/gcc-5.3.0-r0/gcc-5.3.0/gcc/common.md ../../../../../../../work-shared/gcc-5.3.0-r0/gcc-5.3.0/gcc/config/arm/arm.md insn-conditions.md > tmp-automata.c
| make[1]: *** [s-automata] Error 137
| make[1]: *** Waiting for unfinished jobs....
| /bin/bash ../../../../../../../work-shared/gcc-5.3.0-r0/gcc-5.3.0/gcc/../move-if-change tmp-attrtab.c insn-attrtab.c
| /bin/bash ../../../../../../../work-shared/gcc-5.3.0-r0/gcc-5.3.0/gcc/../move-if-change tmp-dfatab.c insn-dfatab.c
| /bin/bash ../../../../../../../work-shared/gcc-5.3.0-r0/gcc-5.3.0/gcc/../move-if-change tmp-latencytab.c insn-latencytab.c
| echo timestamp > s-attrtab
| rm gcc.pod
| make[1]: Leaving directory `/home/jiajizhong/fsl-release-bsp/bld-wayland/tmp/work/x86_64-linux/gcc-cross-initial-arm/5.3.0-r0/gcc-5.3.0/build.x86_64-linux.arm-poky-linux-gnueabi/gcc'
| make: *** [all-gcc] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/jiajizhong/fsl-release-bsp/bld-wayland/tmp/work/x86_64-linux/gcc-cross-initial-arm/5.3.0-r0/temp/log.do_compile.46979)
ERROR: Task 3884 (/home/jiajizhong/fsl-release-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-cross-initial_5.3.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 208 tasks of which 81 didn't need to be rerun and 1 failed.

Outcomes