AnsweredAssumed Answered

Is it possible to capture 1920x1080@60fps video over MIPI CSI-2 on i.mx6 dual or solo?

Question asked by Siddharth Mistry on Dec 22, 2016
Latest reply on Dec 22, 2016 by Siddharth Mistry

Hi

 

From datasheets of i.mx6 dual, it seems to me that it is possible to process following. But, I would like to confirm/clarify the same:

 

[1] Is it possible to capture 1920x1080@60 fps on MIPI CSI-2 (4-lane mode) interface of i.mx6 dual processor?

[2] Is it possible to encode incoming 1920x1080@60 fps video using H.264 encoder and perform following three actions simultaneously?

  1. drop frame rate and encode at 10 fps rate
  2. Stream compressed 1920x1080@10fps video over ethernet with 500us or less latency
  3. store compressed 1920x1080@10fps on local microSD card

[3] Will the i.mx6 solo could take up above mentioned processing load?

 

Please provide your valuable feedback.

 

Regards,

Siddharth Mistry

Outcomes