Hi chip expertise,
When I setup our customer board same schematic with imx6dl sabresd, I got below error.
This means, I have no access read/write the ddrs. Someone can give some debugging method.
load_image u-boot-0x27800000_imx6dl_20160410.bin 0x27800000
JTAG-DP STICKY ERROR
MEM_AP_CSW 0x428000e2, MEM_AP_TAR 0x21b001c
Failed to write memory at 0x021b001c
embedded:startup.tcl:21: Error:
in procedure 'imx6.cpu.0'
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 21
Thanks!
Wenming
Hi wenming
for ocd usage one can check
Using JTAG for imx6 board bringup
Problems in i.mx6 board with openocd
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor!