now i'm blocked by the following error inyocto, when build fsl-image-gui, the do_fetch always be failed.
WARNING: Failed to fetch URL git://git.freescale.com/imx/linux-2.6-imx.git attempting MIRRORS if available.
i have my own kernel image, and don't need bo build this kernel image.
1. so is there some way to build a filesystem without build the kernel image?
i have tried specify the path of my own kernel in linux-imx_3.14.52.bb, but is always failed at do_configure.
Suggest for the Yocto questions, you can check the Yocto project.
If you check the yocto document you can find the command.
http://www.yoctoproject.org/docs/2.2/mega-manual/mega-manual.html
also you can find in the task list.
do_package_setscene Analyzes the content of the holding area and splits it into subsets based on available
...........
.......
do_rootfs Creates the root filesystem (file and directory structure) for an image
do_unpack Unpacks the source code into a working directory
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and all succeeded.
bysun@imx-fae-server-sh:~/yocto/L4.1.15-1.1.0_ga/fsl-release-bsp/imx6ulevk$
after a long wait, now i have passed yocto kernel building, rootfs also is ready.
your respones is very usefull, i will try it later.
many thanks to you.
Hello,
I think, hardly this is possible and makes sense to build system without kernel built.
Regards,
Yuri.
it is very usefull for me, because it is need a very long time to git kernel source from git.freescale.com.
and this kernel is not needed for me,as i have my own kernel.