AnsweredAssumed Answered

LS1043ARDB: Unable to find PCIe endpoint devices

Question asked by ramasubramaniansubramanian on Dec 21, 2016

Hi,

We have got a LS1043ARDB.  We have connected PCI bridge IDT EB-LOGAN-23 evaluation kit.  We have plugged in two endpoint devices to the PCI bridge IDT eval kit.

When we boot up the LS1043ARDB, we only see the IDT EB bridge ports.  We could not see Endpoint devices. We could see the link LEDs glowing on the IDT eval kit.  This setup was working when used with TI Keystone eval kit.

  We are using the default RDB image shipped with the kit. Do we have to do any setup?

lspci

0000:00:00.0 Class 0604: Device 1957:8080 (rev 10)
0001:00:00.0 Class 0604: Device 1957:8080 (rev 10)
0001:01:00.0 Class 0604: Device 111d:808c (rev 02)
0001:02:04.0 Class 0604: Device 111d:808c (rev 02)
0001:02:08.0 Class 0604: Device 111d:808c (rev 02)
0001:02:0c.0 Class 0604: Device 111d:808c (rev 02)
0001:02:10.0 Class 0604: Device 111d:808c (rev 02)
0001:02:14.0 Class 0604: Device 111d:808c (rev 02)

 

Thanks

Rams

Outcomes