AnsweredAssumed Answered

TEST_SEL pin behaviour on T1014

Question asked by Maurizio Cabodi on Dec 20, 2016
Latest reply on Dec 20, 2016 by alexander.yakovlev

Why I should connect the TEST_SEL pin to ground in the T1014 device if I have already bought a T1014?

Does it mean that the device fits two cores? 

If so, after the connection of the pin to ground is the second core disabled/unpowered or what else?

If no, how can I disable the second core on the T1014?

What is the difference in terms of cores between T1024 and T1014?

What is the purpose of TEST_SEL pin?

Is the TEST_SEL pin behaviour equal to other T1/T2/T4 devices?

Thanks

Regards

Outcomes