I have been trying to build core-image-full-cmdline with the latest kernel but I cannot seem to get it to work. The board boots up but nothing is displayed on the screen. In the boot log I am seeing:
Error opening /dev/fb0: No such file or directory
I assume that the driver is not being loaded correctly. I am pulling https://github.com/Freescale/linux-fslc - (branch 4.8.x +fslc) in my recipe. The patch I am applying to the repo is attached. I believe the problem lies in the fact the correct driver is not being loaded. I believe the files in question are the dts files.
The board I am using uses a SMARC card. This is the name of the board SMA-IMX6QI-DVY.
I have attached:
0001-SMARC-revisions.patch - the patch i am applying to the repo
bootlog.txt - the bootlog
Thanks,
Warren
Original Attachment has been moved to: bootlog.txt.zip
Original Attachment has been moved to: 0001-SMARC-revisions.patch.zip
Hi Warren
this may be posted on meta-fsl-arm mailing list, so that someone familiar with
that board could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Latest nxp official bsp is L4.1.15 with documentation located on
i.MX 6 Series Software and Development Tool|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------