Hardware Simulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware Simulator

1,036 Views
jm1015
Contributor II

Is it possible to simulate and test the code for testing peripherals without hardware? My intended processor is P1015/1024 QorIQ processor. I am using GHS multi V7 . Is there any software plug in which help users in develop application before they get actual hardware?

Labels (1)
3 Replies

742 Views
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulators to emulate P1015/1024 peripherals without hardware.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

742 Views
jm1015
Contributor II

Thank you, Alexander.

Is it also not possible to simulate and verify eTSEC module also?

* via loop back

Regards,

J Mathew

0 Kudos

742 Views
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulator to emulate P1015/1024 eTSEC without hardware.