AnsweredAssumed Answered

M_CAN3 ,M_CAN4 Configuration for MPC5777M

Question asked by yalamanda dosakyala on Dec 15, 2016
Latest reply on Dec 22, 2016 by Martin Kovar

Hi All,

Currently we have written can_driver for M_CAN1 and M_CAN2 nodes available on MPC 57xx MB , Now I want to write code for M_CAN3 and M_CAN4, But I am unable to locate the DB-9 Connector type for both M_CAN3 and M_CAN4 and I could n't see it on mother board also.

 

How do I can communicate using M_CAN3 or M_CAN4 and what are Tx and Rx pins for these modules.

 

Is any additional hardware is required to connect to MB ?Martin KovarPetr Stancik

Outcomes