I need CodeWarior 10.6.4 standard edition installation file. I have a license file.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need CodeWarior 10.6.4 standard edition installation file. I have a license file.

1,328 Views
rehan_khan
Contributor III

I need a installation file for CodeWarrior 10.6.4 standard edition. I have a license file for that.

Labels (1)
0 Kudos
2 Replies

1,210 Views
schmark
Contributor I

It appears that the Codewarrior V10.6.4 is no longer posted not available; however, I need to support a project that was built with V10.6.4.  How do I obtain the installation for that version?

0 Kudos

1,272 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rehan,

The installation file is the same for the different License.

Please download it at here :

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos