Hi expert,
Just two simple questions(Platform FRDM-KL43Z, board: MKL43Z256xxx4, SDK 2, KDS: 3.2.0):
1) Does this platform support hardware control (RTS/PTS) for UART? I can see that the MKL43Z4_features.h define the FSL_FEATURE_UART_HAS_MODEM_SUPPORT to 0. So this platform does not support hardware flow control, right?
2) Can I realise a UART with hardware control with FLEXio??
Thanks in advance,
Kaikai
Blue Creation, Cambridge
Hi kaikai,
1) The UART and LPUART module of KL43 doesn't support support hardware flow control (RTS/CTS).
2) The FlexIO module can be used to realize UART hardware flow control (RTS/CTS). For more detail please read the section "39.5.1 UART Transmit" and "39.5.2 UART Receive" in KL43P64M48SF6RM.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------