Hi,
I ve read about setting the TJA1100 in different test modes. But how can I do this?
Is there any strapping I can use or do I connet the PHY to any device for programming the testmode?
Obviously there is an tutorial you can show/give me?
Regards Jerome
Hi Jerome,
The TJA1100 provides five different test modes which can be selected by the extended control bits [8:6]:
A detailed description can be found in the TJA1100 data sheet (page 17). To run a test mode, the TJA1100 must be in Normal mode and LINK_CONTROL must be disabled. In test modes 1-4 the EN pin is reconfigured as output and signals the TX_TCLK clock signal.
Hope it helps.
Best regards,
Tomas
Hi Thomas,
thank you alot. Exactly what I was looking for.
- Do I have to set the modes during startup or do I set the PHY in the test mode while the PHY is in normal mode?
- For the TX_TCLK I have to use the EN pin as CLK-source. Correct?
Best Regards and thank you for your help.
Jérôme