Dear team,
I would like to ask about USB compliance test for i.MX6Q.
My customer wants to know whether there is the test which measure the signals directly from i.MX6Q without using test fixture.
Could you show me if it is possible or not?
Best Regards,
Miyamoto
Hi Igor,
Thanks for your support.
After reading the thread you mentioned, the customer cannot find the way to watch the signals directly without test fixtures.
In that thread the way to use memtool command is also stated but it needs to connect HS device.
Could you show me the concrete way to watch the USB signals directly from i.MX6 without connecting any test fixture or USB devices?
BR,
Miyamoto
Hi Miyamoto
I would suggest to elevate this using local fae channel and ask for on site support .
Best regards
igor
Hi Miyamoto
please check post from "Aug 10, 2015 11:27 PM"
Simple way to do the High Speed Host Electrical Test(including Eye Diagram) without PID/VID Test Fixture:
I.MX6 series USB Certification Guides
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------