AnsweredAssumed Answered

can not disable EMC_CLK in Memory interface for LPC43xx

Question asked by ChungYu Siang on Dec 12, 2016
Latest reply on Jan 3, 2017 by jeremyzhou

Hi,

I'm using LPC4357 256 pin ARM for my embedded system and use an external SDRAM (IS42S16160G).

The SDRAM's clk is connected to CLK1(EMC_CLK1) that is the pin T10. I don't use another CLK Pin such as CLK0, CLK2 and CKL3. The four of clock pins (CLK0 ~ 3) will be enable and set to default value to function 0 as a EMC_CLK output. Actually ,I want to disable the CLK0, 2 and 3 because need to solve EMI/EMC issue. I set the pin function mode to function 2 in CLK0 and CLK2, it could work. Clk0 and Clk2 pin don't have any clock signal now. Unfortunately, when i set the Clk3 to mode 2, the MCU will shutdown even could not enter to main function. I have to pull high the pin ISP Mode Pin, if wanna to program it again. Really confuse about this problem, hope everyone could give me some advice.

 

 

Thank You

Outcomes