Hello!
Can I use VIH(High Level input voltage)/VIL(Low Level input voltage) described in the CLRC663 datasheet as the PDOWN pin specification? The datasheet does not show it clearly.
with best regards,
dee
Solved! Go to Solution.
Hi Dee,
Here is the specification of CLRC663 PDOWN pin:
PDOWN min typ max
VIL low-level input voltage 0 0 0.4
VIH high-level input voltage 0.6 x PVDD VDD(PVDD) VDD(PVDD)
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dee,
Here is the specification of CLRC663 PDOWN pin:
PDOWN min typ max
VIL low-level input voltage 0 0 0.4
VIH high-level input voltage 0.6 x PVDD VDD(PVDD) VDD(PVDD)
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------