AnsweredAssumed Answered

Qt make: g++: Command not found issue with SDK generated for soloX

Question asked by Alankar Dhobale on Dec 9, 2016
Latest reply on Jul 14, 2017 by Daniel Oliveira

i have used following steps to get and build the BSP for soloX sabre board. i am using Krogoth branch to build the bsp and populate sdk

 

GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest 

 

then i added qt support in the build by following 

 

Building Qt5 using yocto on Wandboard - Wandboard Wiki 

 

after that i bitbaked toolchain for this using following

$ bitbake meta-toolchain-qt5

 

after this i generated sdk using following command

 

$ bitbake <image-name> -c populate_sdk

 

and then i installed the sdk on my development machine, it is installed under

/opt/poky/2.1.1/

 

now i installed and setup latest Qt by using following steps

 

Setup QT Creator with Yocto Build 

 

After all this setup done, i created a simple console application and trying to build it, and i get an error as

 

14:10:10: Running steps for project HelloWorld...
14:10:10: Configuration unchanged, skipping qmake step.
14:10:10: Starting: "/usr/bin/make"
g++ -c -pipe -O2 -std=gnu++0x -Wall -W -D_REENTRANT -fPIC -DQT_NO_DEBUG -DQT_CORE_LIB -I../HelloWorld -I. -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include/qt5 -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include/qt5/QtCore -I. -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/lib/qt5/mkspecs/linux-g++ -o main.o ../HelloWorld/main.cpp
make: g++: Command not found
make: *** [main.o] Error 127
14:10:10: The process "/usr/bin/make" exited with code 2.
Error while building/deploying project HelloWorld (kit: mx6solox)
The kit mx6solox has configuration issues which might be the root cause for this problem.
When executing step "Make"
14:10:10: Elapsed time: 00:00.

 

i have googled a lot but could not find any solution on this.

 

Can somebody please help on this...

Outcomes